990-91077K-001

Clearance

NOTE: Clearance dimensions are published for airflow and service access only. Consult with the local safety codes and standards for additional requirements in your local area.
NOTE: If the UPS is installed without side access (Option A*), the length of the cables connected to the UPS must allow for rolling out the UPS.

Clearance for UPS for External Batteries

Option A*

Option B

NOTE: 200 mm left side clearance is required when the UPS is placed next to a wall to allow the front door to open properly.

Clearance for UPS with Internal Batteries

Option A*

Option B

NOTE: 200 mm left side clearance is required when the UPS is placed next to a wall to allow the front door to open properly.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.