990-91077K-001

Electrolyte Values for Modular Battery Cabinet and UPSs with Internal Batteries

Commercial Reference Description Electrolyte Volume L (gal) Electrolyte Weight kg (lbs)
E3SBTU Standard battery module 3.780 (1) 5 (11.1)
E3SBT4 Standard battery string 15.120 (4) 20 (44.4)
E3SBTHU High performance battery module 3.330 (0.9) 4.4 (9.8)
E3SBTH4 High performance battery string 13.320 (3.6) 17.6 (39.2)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.