990-91077K-001

Battery Gassing Rates for Modular Battery Cabinets and UPSs with Internal Batteries

The battery gassing rates are calculated based on:

  • Gassing Rate at 2.4 V/cell (ft3 /hr) assuming 97% recombination efficiency

  • Six cells per battery module

  • Ten batteries per cartridge

Commercial Reference Description Typical cm³/hr (ml/hr)
E3SBTU Standard battery module 10.73 (10.73)
E3SBT4 Standard battery string 42.93 (42.93)
E3SBTHU High performance battery module 12.67 (12.67)
E3SBTH4* High performance battery string 50.68 (50.68)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.