990-91077K-001

Heat Dissipation for 400 V Systems

  10 kVA 15 kVA 20 kVA 30 kVA 40 kVA
Normal mode (W) 516 852 870 1410 1810
Battery mode (W) 600 950 1080 1700 2270
ECO mode (W) 135 223 240 370 480
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.