990-91077K-001

Heat Dissipation for 208 V Systems

  10 kVA 15 kVA 20 kVA
Normal mode (W) 920 1469 1701
Battery mode (W) 948 1247 1861
ECO mode (W) 245 358 415
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.