990-91077K-001

Input Power Factor

Input Power Factor – 3:3 UPSs

The values are at 208 V, 60 Hz load.

  10 kVA 15 kVA 20 kVA
25% load 0.98 0.99 0.97
50% load 0.99 0.99 0.99
75% load 0.99 0.99 0.99
100% load 0.99 0.99 0.99
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.