990-91077K-001

Airflow Requirement for 400 V Systems

NOTE: The UPS requires a sufficient amount of fresh air in the installation room.
  10 kVA 15 kVA 20 kVA 30 kVA 40 kVA
Fan air throughput (m³/min) 6.20 8.25 10.85 15.57 16.38
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.