990-5910G-001

Configure High Efficiency Mode

  1. Tap Configuration > High efficiency.
  2. Select the High efficiency mode: Disable, ECO mode, or eConversion.
    NOTE: Contact Schneider Electric to enable ECO mode.
  3. Select eConversion harmonics compensator, if relevant.
  4. Select the High efficiency schedule: Active on schedule, Always active, or Never active.
    1. For Active on schedule, tap Schedule and set up and enable the schedule(s) as needed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.