Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
![]() |
---|
DANGER indicates a hazardous situation which, if
not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
WARNING indicates a hazardous situation which,
if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
![]() |
---|
CAUTION indicates a hazardous situation which,
if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
|
NOTICE |
---|
NOTICE is used to address practices not related
to physical injury. The safety alert symbol shall not be used with
this type of safety message.
Failure to follow these instructions can result in equipment damage.
|
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.
The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040-1, section 3.102).
FCC Statement
Any changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.
Electromagnetic Compatibility
NOTICE |
---|
Risk of electromagnetic disturbance
This is a product category C2 UPS product. In a residential
environment, this product may cause radio inference, in which case
the user may be required to take additional measures.
Failure to follow these instructions can result in equipment damage.
|
Safety Precautions
![]() |
---|
hazard of electrical shock, explosion or arc flash
All safety instructions in this document must be read,
understood and followed.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
hazard of electrical shock, explosion or arc flash
After the UPS system has been electrically wired, do not
start up the system. Start-up must only be performed by Schneider
Electric.
Failure to follow these instructions will result in death or serious injury.
|