990-5910G-001

Transfer the UPS from Normal Operation to Static Bypass Operation

  1. Select Control > Operation mode > Transfer to bypass operation.
  2. Tap OK on the confirmation screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.