Start a Runtime Calibration Test
This feature is used for calibrating the estimated remaining battery runtime value. In this test, the UPS transfers to battery operation and the batteries are discharged to the low DC warning level. Based on the elapsed time and information about the load, the battery capacity can be calculated and the estimated runtime calibrated.
Schneider Electric recommends performing a runtime calibration test at start-up, when batteries are replaced, or when changes are made to the battery solution.
| NOTICE |
|---|
|
risk of equipment damage
Failure to follow these instructions can result in equipment damage.
|
Prerequisites:
-
No critical alarms present.
-
Batteries must be 100% charged.
-
The load percentage must be at least 10% and must not change more than 20% during the test. Example: If the load percentage is 30% at the start of the test, the test will abort if the load percentage drops below 24% or rises above 36% during the test.
-
The bypass supply must be available.
-
The operation mode must be normal operation, eConversion, or ECO mode.
-
The system operation mode must be inverter, eConversion, or ECO mode.
- Tap the menu button on the home screen.
- Select .
- Tap OK on the confirmation screen.