990-5910F-001

Connect Temperature/Humidity Sensor (Option)

Temperature/humidity sensor (AP9335T or AP9335TH) can be connected to the network management card.

  1. Connect the temperature/humidity sensor to the universal I/O port of the network management card.
  2. Set up the temperature/humidity sensor via the network management interface, see Access a Configured Network Management Interface.
  3. To see the temperature/humidity measurements, tap Status > Temperature.
QR code for this page

Was this helpful?