990-5910G-001

Enable HTTP/HTTPS Protocols

  1. Access the network management interface by its IP address (or its DNS name, if a DNS name is configured).
  2. Enter the user name and password. The default user name and password is apc. You will be prompted to change this password on the first login.
  3. To enable or disable the HTTP or HTTPS protocol, go to Configuration > Network > Web > Access, select the protocol, set the parameters, and click on Apply.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?