View the System Status Information
- Tap Status.
- Tap Input, Output, Bypass, Battery, Temperature, or Parallel to see
                        the status. 
Input
Voltage ph-ph (phase-to-phase) The present phase-to-phase input voltage. Current The present input current from the AC utility power source per phase in amperes (A). Frequency The present input frequency in hertz (Hz). Voltage ph-N (phase-to-neutral)* The present phase-to-neutral input voltage in volts (V). Total power The present total active power input (for all three phases) in kW. Power The present active power (or real power) input for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction. Peak current The input peak current in amperes (A). Power factor The ratio of the active power to apparent power. Max. RMS current The present maximum RMS current. Energy The total energy consumption since the time of installation. Output
Voltage ph-ph (phase-to-phase) The phase-to-phase output voltage at the inverter in volts (V). Current The present output current for each phase in amperes (A). Frequency The present output frequency in hertz (Hz). Voltage ph-N (phase-to-neutral)* The phase-to-neutral output voltage at the inverter in volts (V). Load The percentage of the UPS capacity presently used across all phases. The load percentage for the highest phase load is displayed. Neutral current* The present output neutral current in amperes (A). Total power The present active total output power (for all three phases) in kilowatts (kW). Power The present active power (or real power) output for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction. Peak current The output peak current in amperes (A). Power factor The present output power factor for each phase. Power factor is the ratio of active power to apparent power. Max. RMS current The present maximum RMS current. Energy The total energy supplied since the time of installation. Crest factor The present output crest factor for each phase. The output crest factor is the ratio of the peak value of the output current to the RMS (root mean square) value. Bypass
Voltage ph-ph (phase-to-phase) The present phase-to-phase bypass voltage (V). Current The present bypass current for each phase, in amperes (A). Frequency The present bypass frequency in hertz (Hz). Voltage ph-N (phase-to-neutral)* The present phase-to-neutral bypass voltage (V). Total power The present total active bypass power (for all three phases) in kilowatts (kW). Power The present active bypass power for each phase in kilowatts (kW). Active power is the time average of the instantaneous product of voltage and current. Peak current The bypass peak current in amperes (A). Power factor The present bypass power factor for each phase. Power factor is the ratio of active power to apparent power. Max. RMS current The present maximum RMS current. Battery
Measurements The present DC power being drawn from the battery, in kilowatts (kW). The present battery voltage (VDC). The present battery current in amperes (A). A positive current indicates that the battery is charging; a negative current indicates that the battery is discharging. Battery temperature from the connected temperature sensors in Celsius or Fahrenheit. Battery The amount of time before the batteries reach the low-voltage shutdown level. Also shows charge level of the battery as a percentage of full charge capacity. The present battery charge (Ah). Configuration Shows battery type. For a modular battery, tap the Details button in this field to see the modular battery details. See View the Modular Battery Status. Status The general condition of the charger. Mode The operation mode of the charger (Off, Float, Boost, Equalization, Cyclic, Test). Charging capacity The maximum charge capacity in percentage of the UPS nominal power rating. Temperature
Ambient temperature Ambient temperature in Celsius or Fahrenheit. Battery temperature Battery temperature in Celsius or Fahrenheit from the connected battery temperature sensors. Temperature Ambient temperature in Celsius or Fahrenheit from the optional connected temperature sensors (AP9335T and AP9335TH). Naming to be set up via the network management interface. Humidity Humidity in percentage from the optional connected humidity sensors (AP9335TH). Naming to be set up via the network management interface. Parallel
Input current The present input current from the input source per phase in amperes (A). Bypass current The present bypass current from the bypass source per phase in amperes (A). Total output power The total output power of the parallel UPS system showing the total load percentage and the total output power in kW and kVA for the parallel system. Output current The present output current for each phase in amperes (A). Number of redundant UPSs The number of redundant UPSs present. Redundancy setting The configured redundancy setting.  
 - Tap Input, Output, Bypass, Battery, Temperature, or Parallel to see
                        the status.