990–5809D-006

Galaxy VXSAI de 400/480 V con armario de E/S de 1000 kWInstalación

300 kW/kVA, 300 kW/kVA N+1,
400 kW/kVA, 400 kW/kVA N+1,
500 kW/kVA, 500 kW/kVA N+1,
625 kW/kVA, 625 kW/kVA N+1,
500 kW/kVA ampliable a 750 kW/kVA, 750 kW/kVA, 750 kW/kVA N+1,
500 kW/kVA ampliable a 1000 kW/kVA, 625 kW/kVA ampliable a 1000 kW/kVA,
750 kW/kVA ampliable a 1000 kW/kVA, 1000 kW/kVA, 1000 kW/kVA N+1

10/2019

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

¿Le ha resultado útil?