990–5809D-001

Galaxy VXUPS with 1000 kW I/O Cabinet 400/480 VInstallation

300 kW/kVA, 300 kW/kVA N+1,
400 kW/kVA, 400 kW/kVA N+1,
500 kW/kVA, 500 kW/kVA N+1,
625 kW/kVA, 625 kW/kVA N+1,
500 kW/kVA Expandable to 750 kW/kVA, 750 kW/kVA, 750 kW/kVA N+1,
500 kW/kVA Expandable to 1000 kW/kVA, 625 kW/kVA Expandable to 1000 kW/kVA,
750 kW/kVA Expandable to 1000 kW/kVA, 1000 kW/kVA, 1000 kW/kVA N+1

10/2019

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?