990–5809D-018

Galaxy VX1000 kW 400/480 V I/Oキャビネット搭載UPS設置マニュアル

300 kW/kVA、300 kW/kVA N+1、
400 kW/kVA、400 kW/kVA N+1、
500 kW/kVA、500 kW/kVA N+1、
625 kW/kVA、625 kW/kVA N+1、
500 kW/kVA(750 kW/kVAに拡張可能)、750 kW/kVA、750 kW/kVA N+1、
500 kW/kVA(1000 kW/kVAに拡張可能)、625 kW/kVA(1000 kW/kVAに拡張可能)、
750 kW/kVA(1000 kW/kVAに拡張可能)、1000 kW/kVA、1000 kW/kVA N+1

2019年10月

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

この情報は役に立ちましたか?