990-5452N-001

Change the System Names

  1. From the home screen on the display select Configuration > Customer > ID Setup.
  2. The following names can be changed.
    • UPS

    • Input

    • System Output

    • Maintenance Bypass

    • Bypass

    • System Bypass

  3. Tap OK to confirm your settings.
  4. Tap the home button to exit the configuration screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.