990-5452N-001

Connect to the 10” System Bypass Display Remotely

  1. In Internet Explorer 10 or newer, type in the IP address of the display. If you want to disable this feature, ensure that the IP address of the display is left blank.
  2. If requested, follow Active X installation instructions.
  3. Select the Monitoring tab and then select Web Gate > New Window in the left pane.
    You now have access to the status and log information of the parallel system.
  4. Log in with your username and password. Please ensure that you change your password before using the remote feature in order to secure your connection. It is recommended to change your password regularly.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.