990-5452N-001

Configure the Output Distribution Disconnect Devices

  1. From the home screen on the display select Configuration > Customer > Output Setup.
  2. Select Present for the output distribution disconnect devices that are available in the parallel system.
  3. Select Present for the Load Bank Breaker if it is part of the parallel system and indicate whether the load bank disconnect device is Upstream of SIB or Downstream of SIB.
  4. Tap OK to confirm your settings.
  5. Tap the home button to exit the configuration screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.