990-5452N-001

Tests

The UPS system can perform the following tests to ensure correct performance of the system:

  • Battery Test

  • Runtime Calibration

  • Battery SPoT Mode

  • Annunciators

  • Display Calibration

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.