990-5452N-001

View the Parallel System Status

  1. From the home screen on the display select Status > Parallel System.
  2. Select the area for which you wish to see the status. Choose between:

    Measurements

    Input Current (A)

    The present phase-to-phase input current in amperes (A).

    Output Current (A)

    The present phase-to-phase output current in amperes (A).

    Bypass Current (A)

    The present phase-to-phase bypass current in amperes (A).

    Number of Parallel UPS

    The total number of UPSs in the parallel system.

    Number of Redundant UPS

    The redundancy for the parallel system.

    Number of Redundant Power Cabinets per UPS

    The number of redundant power cabinets in each UPS.

    Output Total Apparent Power (kVA)

    The present total apparent output power (for all three phases) in thousands of Volt-Amps (kVA).

    Output Total Active Power (kW)

    The present total active output power (for all three phases) in kilowatts (kW).

    Output Total Load (%)

    The percentage of the UPS system capacity presently used across all phases. The load percentage for the highest phase load is displayed.

    Mimic Diagram

    Mimic Diagram

    The mimic diagram shows the current status of the main parts of the UPS system: power sources, converters, bypass static switch and disconnect devices, and it shows the power flow through the system.

    NOTE: You can click the UPS or the system bypass to get a more detailed mimic diagram.

    Communication Status

    Communication Status

    The communication status diagram shows the communication status between the display and the UPSs of the parallel system.

  3. Tap the home button to exit the screens and return to the home screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.