990-5452N-001

Transfer UPS from Requested Static Bypass Operation to Normal Operation

  1. From the home screen on the display select Control > Operational Mode.
  2. Tap the Transfer to Inverter Operation button.
    NOTE: If the conditions for performing a transfer are not met, the button will be grayed out.
  3. Verify that the UPS Operation Mode changes to Normal Operation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.