990-5452N-001

Calibrate the Display

From the home screen on the display select Tests > Display Calibration and then select the calibration you want to perform.

  • Calibrate: Tests and adjusts the touch screen target sensitivity.

  • Calibration Check: Checks the calibration adjustments.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.