990-5452N-001

Shut Down Single System from Normal to Maintenance Bypass Operation

Use this procedure to shut down a single system to maintenance bypass operation with the load supplied through the MBB.

NOTE: Only operate a disconnect device when the associated disconnect device LED is green.
  1. From the home screen on the display, select Control > Shutdown Wizard. Select Shutdown ending in Maintenance Bypass and follow the steps which appear on the screen.
    NOTE: The following is a generic shutdown procedure. Always follow the steps of the Shutdown Wizard which are specific to your system.
  2. Initiate transfer to static bypass by tapping the Transfer Load to static bypass button on the display interface.

    In systems with kirk-keys, the key is released from the solenoid key release unit.

    If the UPS system does not transfer to requested static bypass, go to Status > Active Alarms to see if there are active alarms that prevent the UPS system from transferring to static bypass.

  3. In systems with kirk-keys, insert the key in the lock on MBB and turn to unlock.
  4. Close MBB.
    In systems with kirk-keys, the key is held in the lock.
  5. Open UOB.
  6. In systems with kirk-keys, turn the key in the lock on the unit output breaker UOB to lock open.
    The key is released.
  7. In systems with kirk-keys, insert the key in the solenoid key release unit and turn to capture the key.
  8. Open SSIB.
  9. Initiate transfer to forced static bypass by tapping the Inverter OFF button on the front of the UPS system.
  10. Open the battery disconnect devices in your specific battery solution.
  11. Open UIB.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.