990-5452N-001

Configure the Output Relays

  1. On the display select Configuration > Output Relays.
  2. Select to enable or disable Energized check mode.
    • When Energized check mode is enabled the output relays are ON. If a signal is received or the power supply to the relay is lost, the circuit will open and the relay will be deactivated.
    • When Energized check mode is disabled the output relays are OFF. If a signal is received, the circuit will close and the relay will be activated.
  3. Select the output relay that you wish to configure.
  4. Select the function that you wish to use the specific output relay for from the list below:

    Common Alarm: The output is triggered when any alarm is present.

    Normal Operation: The output is triggered when the UPS is running in normal operation.

    Battery Operation*: The output is triggered when the UPS is running in battery operation.

    Maintenance Bypass*: The output is triggered when the UPS is running in maintenance bypass operation.

    Static Bypass*: The output is triggered when the UPS is running in forced static bypass operation or requested static bypass operation.

    High Efficiency Mode: The output is triggered when the UPS is running in eConversion or ECO mode.

    Output Overload: The input is triggered when there is an overload condition.

    Fan Inoperable: The output is triggered when one or more fans are inoperable.

    Battery is not Working Correctly*: The output is triggered when the batteries are not working correctly.

    Battery Disconnected*: The output is triggered when the batteries have been disconnected or the battery disconnect device(s) are open.

    Battery Voltage Low*: The output is triggered when the battery voltage is below the threshold.

    Input Out of Tolerance: The output is triggered when the input is out of tolerance.

    Bypass Out of Tolerance*: The output is triggered when the bypass is out of tolerance.

    UPS Warning: The output is triggered when a warning alarm is present.

    UPS Critical: The output is triggered when a critical alarm is present.

    Parallel Redundancy Lost: The output is triggered when the specified redundancy has been lost.

    External Fault: The output is triggered when a fault external to the UPS is present.

    UPS Maintenance Mode: The output is triggered when the unit output disconnect device (UOB) is open.

    System Warning: The output is triggered when a warning alarm is present in a parallel system.

    System Critical: The output is triggered when a critical alarm is present in a parallel system.

    System Common Alarm: The output is triggered when any alarm is present in a parallel system.

    Emergency power off activated: The output is triggered when the EPO has been activated.

    Transfer to static bypass disabled

    UPS informational alarm: The output is triggered when an information alarm is present.

    System informational alarm: The output is triggered when an information alarm is present in a parallel system.

     
  5. Set the delay in seconds for the specific output to activate. Select a value between 0 and 60 seconds.
  6. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.