990-5452N-001

Configure the Display Settings

  1. From the home screen on the display select Configuration > Display > System Settings.
  2. Set the Alarm Volume. Choose between: Off, Low, Medium, and High.
  3. Set the Button Volume. Choose between: Off, Low, Medium, and High.
  4. Set the Brightness of the display. Choose between: Low, Medium, and High.
  5. Enable or disable Backlight Timeout. If you wish to enable backlight timeout, set the time limit in minutes for enabling backlight timeout. Choose between: 60, 30, 10, 5, and 1.
  6. Set the intensity of the backlight. Choose between: Off, Very Low, Low, and Medium.
  7. Set the time limit in minutes for automatic log off. Choose between: 60, 30, 10, 5, and 1.
  8. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.