990-5452N-001

View UPS Status Information

  1. From the home screen on the display select Status > UPS X.
  2. Select the area for which you wish to see the status. Choose between:

    Input

    Voltage (V) phase-to-neutral*

    The present phase-to-neutral input voltage in volts (V).

    Current (A)

    The present input current from the AC utility power source per phase in amperes (A).

    Peak RMS Current (A)

    The maximum current for the latest 30 days.

    Apparent Power (kVA)

    The present apparent input power for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Active Power (kW)

    The present active input power (or real power) for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.

    Power Factor

    The ratio of the active power to apparent power.

    Voltage (V) phase-to-phase

    The present phase-to-phase input voltage.

    Total Apparent Power (kVA)

    The present total apparent input power (for all three phases) in kVA.

    Total Active Power (kW)

    The present total active input power (for all three phases) in kW.

    Frequency (Hz)

    The present input frequency in hertz (Hz).

    Energy (kWh)

    The total energy consumption since the time of installation or since the number was reset.

    Output

    Voltage (V) phase-to-neutral*

    The phase-to-neutral output voltage at the inverter in volts (V).

    Current (A)

    The present output current for each phase in amperes (A).

    Peak RMS Current (A)

    The maximum current for the latest 30 days.

    Apparent Power (kVA)

    The present apparent output power for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Active Power (kW)

    The present active output power (or real power) for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.

    Power Factor

    The present output power factor for each phase. Power factor is the ratio of active power to apparent power.

    Current Crest Factor

    The present output crest factor for each phase. The output crest factor is the ratio of the peak value of the output current to the RMS (root mean square) value.

    Current THD (%)

    The THD (total harmonic distortion) for each phase, as a percentage, for the present output current.

    Voltage (V) phase-to-phase

    The phase-to-phase output voltage at the inverter in volts (V).

    Total Apparent Power (kVA)

    The present apparent output power for each phase in thousands of Volt-Amps (kVA). Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Total Active Power (kW)

    The present total active output power (for all three phases) in kilowatts (kW).

    Load (%)

    The percentage of the UPS capacity presently used across all phases. The load percentage for the highest phase load is displayed.

    Neutral Current (A)1

    The present output neutral current in amperes (A).

    Frequency (Hz)

    The present output frequency in hertz (Hz).

    Inverter Status

    The general condition of the inverter.

    PFC Status

    The general condition of the PFC.

    Energy (kWh)

    The total energy supplied since the time of installation or since the value was reset.

    Bypass

    Voltage (V) phase-to-neutral*

    The present phase-to-neutral bypass voltage (V).

    Current (A)

    The present bypass current for each phase, in amperes (A).

    Peak RMS Current (A)

    The maximum current for the latest 30 days.

    Apparent Power (kVA)

    The present apparent bypass power for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Active Power (kW)

    The present active bypass power for each phase in kilowatts (kW). Active power is the time average of the instantaneous product of voltage and current.

    Power Factor

    The present bypass power factor for each phase. Power factor is the ratio of active power to apparent power.

    Voltage (V) phase-to-phase

    The present phase-to-phase bypass voltage (V).

    Total Apparent Power (kVA)

    The present total apparent bypass power (for all three phases) in thousands of Volt-Amps (kVA).

    Total Active Power (kW)

    The present total active bypass power (for all three phases) in kilowatts (kW).

    Frequency (Hz)

    The present bypass frequency in hertz (Hz).

    Battery

    Voltage (V)

    The present battery voltage.

    Current (A)

    The present battery current in amperes (A).

    A positive current indicates that the battery is charging; a negative current indicates that the battery is discharging.

    Power (kW)

    The present DC power being drawn from the battery, in kilowatts (kW).

    Estimated Charge Level (%)

    The present battery charge, as a percentage of full charge capacity.

    Estimated Charge Time (h:mn)

    The estimated time, in minutes, until the batteries reach 100% charge.

    Runtime Remaining (h:mn)

    The amount of time in hours and minutes before the batteries reach the low-voltage shutdown level.

    Charger Mode

    The operation mode of the charger (Off, Float, Boost, Equalization, Cyclic, Test).

    Battery Status

    The general condition of the battery.

    Charger Status

    The general condition of the charger.

    Total Battery Capacity (Ah)

    The total capacity available from the available batteries.

    Battery Temperature C°

    The highest battery temperature from the connected temperature sensors.

    Temperature

    Temperature

    Ambient temperature in degrees Celsius or Fahrenheit for the I/O cabinet and each power cabinet.

    System

    Output Voltage

    The phase-to-phase output voltage at the inverter in volts (V).

    Output Current

    The present output current for each phase in amperes (A).

    Output Frequency

    The present output frequency in hertz (Hz).

    Runtime Remaining

    The amount of time in hours and minutes before the batteries reach the low-voltage shutdown level.

    System Time

    The time of the UPS system.

    UPS Operation Mode

    The operation mode of the operated UPS.

    System Operation Mode

    The operation mode of the complete UPS system.

    Total Output Power

    The apparent and active power (or real power) output for each phase.

    Output Power

    The phase-to-phase apparent and active output power (or real power) for each phase.

    Mimic Diagram

    Mimic Diagram

    The mimic diagram shows the current status of the main parts of the UPS: power sources, converters, bypass static switch and disconnect devices, and it shows the power flow through the UPS.

    Detailed View

    Detailed view

    The detailed view shows the system with a status icon on each individual power cabinet and the actual number of redundant power cabinets. The detailed view also shows the apparent power and active power per phase.

  3. Tap the home button to exit the screens and return to the home screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.