990-5452N-001

Configure the Display Settings

  1. From the home screen on the display select Configuration > Display.
  2. Set the brightness of the display via the Brightness indicator. Tap + to increase the brightness and tap to decrease the brightness.
  3. Set the backlight timeout. Choose between 1, 2, 5, 10, 15, or 30 minutes.
  4. Set the language of the display.
  5. Configure the network by tapping the Network configuration button and typing in the IP Address, Mask, and Gateway. Complete with OK.
  6. Tap the home button to exit the configuration screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.