990-5452N-001

Logs

There are two types of logs:

  • NMC Log: Contains information about the display and network activities.

  • UPS Log: Contains information about the system status and operation modes.

View the NMC Log

  1. From the home screen on the display select Logs > NMC Log.
  2. You can browse through the list of the events using the arrows.
  3. You can now perform the following operations in the event log:
    1. Tap the filter button to filter the events. Different filter settings are available, including:

      Filters for Power Events: Communication, Device, Output, Input, Battery, UPS Operation Mode, Parallel System, Reminders, Switchgear, and/or RFC 1628 MIB.

      Filters for System Events: Mass Configuration and/or Security.

    2. Tap the recycle bin button to clear the event log and select Yes to confirm.
  4. Tap the home button to exit the log.

View the UPS Log

  1. From the home screen on the display select Logs > UPS Log.
  2. You can now browse through the list of the UPS events using the arrows.
  3. You can perform the following operations in the UPS log:
    1. Tap the filter button to filter the events. Different filter settings are available, including:

      Filters for Power Events: Communication, Device, Output, Input, Battery, UPS Operation Mode, Parallel System, Reminders, Switchgear, and/or RFC 1628 MIB.

      Filters for System events: Mass Configuration and/or Security.

    2. Tap the recycle bin button to clear the UPS log and select Yes to confirm.
  4. Tap the home button to exit the log.

Export Data from Logs

The exported log can only be used by Schneider Electric customer support for analysis.

  1. From the home screen on the display select Logs > Export Data.
  2. Insert a USB device in the USB port (A) located on the front of the display.

    Display Model 1

    Display Model 2

  3. Tap the Start Data Export button.

    When the download is complete, the following message will be shown on the screen: Data Exported Successfully. Remove USB device.

  4. Remove the USB device and tap the home button to exit the screen.
  5. The exported data on the USB device can now be sent to Schneider Electric support for analyzing.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.