990-5452N-001

View the System Status Information

NOTE: The display does not show real time data, and a comparison between the display and an external power analyzer will not show the same data. Please allow for a tolerance of ± 1% for voltages, ± 3% for power, and ± 3% for currents.
  1. From the home screen on the display select Status.
  2. Select the area for which you wish to see the status. Choose between:

    Input

    Voltage (phase-to-neutral)*

    The present phase-to-neutral input voltage in volts (V).

    Current

    The present input current from the AC utility power source per phase in amperes (A).

    Maximum RMS Current

    The maximum current for the latest 30 days.

    Apparent Power

    The present apparent power input for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Active Power

    The present active power (or real power) input for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.

    Power Factor

    The ratio of the active power to apparent power.

    Voltage (phase-to-phase)

    The present phase-to-phase input voltage.

    Total Apparent Power

    The present total apparent power input (for all three phases) in kVA.

    Total Active Power

    The present total active power input (for all three phases) in kW.

    Frequency

    The present input frequency in hertz (Hz).

    Energy

    The total energy consumption since the time of installation or since the number was reset.

    Output

    Voltage (phase-to-neutral)*

    The phase-to-neutral output voltage at the inverter in volts (V).

    Current

    The present output current for each phase in amperes (A).

    Maximum RMS Current

    The maximum current for the latest 30 days.

    Apparent Power

    The present apparent power output for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Active Power

    The present active power (or real power) output for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.

    Power Factor

    The present output power factor for each phase. Power factor is the ratio of active power to apparent power.

    Current Crest Factor

    The present output crest factor for each phase. The output crest factor is the ratio of the peak value of the output current to the RMS (root mean square) value.

    Current THD

    The THD (total harmonic distortion) for each phase, as a percentage, for the present output current.

    Voltage (phase-to-phase)

    The phase-to-phase output voltage at the inverter in volts (V).

    Total Apparent Power

    The present apparent power output for each phase in thousands of Volt-Amps (kVA). Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Total Active Power

    The present total active output power (for all three phases) in kilowatts (kW).

    Load

    The percentage of the UPS capacity presently used across all phases. The load percentage for the highest phase load is displayed.

    Neutral Current*

    The present output neutral current in amperes (A).

    Frequency

    The present output frequency in hertz (Hz).

    Inverter Status

    The general condition of the inverter.

    PFC Status

    The general condition of the PFC.

    Energy

    The total energy supplied since the time of installation or since the value was reset.

    Bypass

    Voltage (phase-to-neutral)*

    The present phase-to-neutral bypass voltage (V).

    Current

    The present bypass current for each phase, in amperes (A).

    Maximum RMS Current

    The maximum current for the latest 30 days.

    Apparent Power

    The present apparent bypass power for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Active Power

    The present active bypass power for each phase in kilowatts (kW). Active power is the time average of the instantaneous product of voltage and current.

    Power Factor

    The present bypass power factor for each phase. Power factor is the ratio of active power to apparent power.

    Voltage (phase-to-phase)

    The present phase-to-phase bypass voltage (V).

    Total Apparent Power

    The present total apparent bypass power (for all three phases) in thousands of Volt-Amps (kVA).

    Total Active Power

    The present total active bypass power (for all three phases) in kilowatts (kW).

    Frequency

    The present bypass frequency in hertz (Hz).

    Battery

    Voltage

    The present battery voltage.

    Current

    The present battery current in amperes (A).

    A positive current indicates that the battery is charging; a negative current indicates that the battery is discharging.

    Power

    The present DC power being drawn from the battery, in kilowatts (kW).

    Estimated Charge Level

    The present battery charge, as a percentage of full charge capacity.

    Estimated Charge Time

    The estimated time, in minutes, until the batteries reach 100% charge.

    Runtime Remaining

    The amount of time in hours and minutes before the batteries reach the low-voltage shutdown level.

    Charger Mode

    The operation mode of the charger (Off, Float, Boost, Equalization, Cyclic, Test).

    Battery Status

    The general condition of the battery.

    Charger Status

    The general condition of the charger.

    Total Battery Capacity

    The total capacity available from the available batteries.

    Temperature

    The highest battery temperature from the connected temperature sensors.

    Temperature

    Ambient Temperature

    Ambient temperature in degrees Celsius or Fahrenheit for the I/O cabinet and each power cabinet.

    System

    Output Voltage

    The phase-to-phase output voltage at the inverter in volts (V).

    Output Current

    The present output current for each phase in amperes (A).

    Output Frequency

    The present output frequency in hertz (Hz).

    Runtime Remaining

    The amount of time in hours and minutes before the batteries reach the low-voltage shutdown level.

    System Time

    The time of the UPS system.

    UPS Operation Mode

    The operation mode of the operated UPS.

    System Operation Mode

    The operation mode of the complete UPS system.

    Total Output Power

    The apparent and active power (or real power) output for each phase.

    Overload Timer*

    The time in seconds before the UPS changes to forced static bypass due to an overload condition on the system.

    NOTE: The system can be in an overload condition even though the Total Output Power is below 100% if the load is not equally shared between the three phases.

    Output Power

    The phase-to-phase apparent and active power (or real power) output for each phase.

    Parallel System

    Input Current

    The present phase-to-phase input current in amperes (A).

    Output Current

    The present phase-to-phase output current in amperes (A).

    Bypass Current

    The present phase-to-phase bypass current in amperes (A).

    Parallel UPS Number

    The parallel UPS number of the operated UPS.

    Parallel system redundancy

    The redundancy for the parallel system.

    Number of Parallel Units

    The total number of UPSs in the parallel system.

    Parallel Units

    The numbers of all UPSs in the parallel system.

    Output Total Apparent Power

    The present total apparent output power (for all three phases) in thousands of Volt-Amps (kVA).

    Output Total Load

    The percentage of the UPS system capacity presently used across all phases. The load percentage for the highest phase load is displayed.

    Active Alarms

    Active Alarms

    For more information on active alarms, go to View the Active Alarms.

    Mimic Diagram

    Mimic Diagram

    The mimic diagram shows the current status of the main parts of the UPS system: power sources, converters, bypass static switch and disconnect devices, and it shows the power flow through the system.

    Detailed View

    Detailed view

    The detailed view shows the system with a status icon on each individual power cabinet and the actual number of redundant power cabinets. The detailed view also shows the apparent power and active power per phase.

    Symbols on the Detailed View Screen

    Indicates that the power cabinet is operational and working correctly
    Indicates that there is an informational alarm.
    Indicates that the power cabinet redundancy has been lost and/or an alarm of severity level Warning is present in the power cabinet. The power cabinet is still operational.
    Indicates that the power cabinet is inoperable due to a critical event. The customer alarm Power cabinet inoperable is also displayed.

    Peak Shaving Mode

    Peak shaving mode

    The status of the peak shaving mode — Active or Inactive

    Input power

    The present input power (kW).

    Battery power

    The present battery power (kW). The bar is green when the batteries are charging and yellow when the batteries are discharging.

    Peak shaving

    Indicates if the charger is enabled or disabled and if forced battery operation is enabled or disabled.

    State of charge

    The current charge status of the batteries.

    Remaining time

    The remaining time in battery operation and peak shaving mode.

  3. Tap the home button to exit the screens and return to the home screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.