990-5452N-001

Configure High Efficiency Mode

NOTE: ECO Mode must be enabled by Schneider Electric during service configuration to make this selection available.

The UPS returns to high efficiency mode after 10 seconds under normal operating conditions. If an unstable mains forces the UPS to exit high efficiency mode more than one to ten times (this setting must be configured by Schneider Electric) within 24 hours, the UPS will disable high efficiency mode. An informational alarm will be generated, and Disabled by system will be shown on the screen Configuration > UPS > High Efficiency Mode. High efficiency must then be manually reactivated.

  1. From the home screen on the display select Configuration > UPS > High Efficiency Mode and configure the following settings:
    1. Select High Efficiency Mode: Choose between Disable, ECO Mode, eConversion, and eConversion Harmonics Compensator.
  2. Tap > and configure the schedule settings:
    1. Schedule: Select when the system should enter the selected eConversion or ECO mode. Choose between Always, Programmed and Never.
    2. Active Schedules List: If you chose Programmed above, select Enable and set the time and date for when the system should enter the selected eConversion or ECO mode.
  3. Tap OK to confirm your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.