990-6264F-018

Galaxy VX1250 kW I/Oキャビネット搭載UPS設置マニュアル

380 V、400 V、415 V、440 V、480 V

500 kW/kVA、500 kW/kVA N+1、625 kW/kVA、800 kW/kVA
500 kW/kVA(750 kW/kVAに拡張可能)、750 kW/kVA、750 kW/kVA N+1
500 kW/kVA、625 kW/kVA、750 kW/kVA(1000 kW/KVAに拡張可能)、1000 kW/kVA、1000 kW/kVA N+1
1100 kW/kVA、1100 kW/kVA N+1
500 kW/kVA、750 kW/kVA、1000 kW/kVA(1250 kW/kVAに拡張可能)、1250 kW/kVA、1250 kW/kVA、1250 kW/kVA N+1

2024年11月

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

この情報は役に立ちましたか?