About the Book
Document Scope
This manual describes the configuration and usage of Harmony BX1 with the product version (PV) 02 or lower.
Harmony BX1 is designed to operate in an industrial environment.
| NOTICE |
|---|
|
UNINTENDED PRODUCT USAGE
Check the product version in use and the Harmony BX1 User
Guide for the product version.
Failure to follow these instructions can result in equipment damage.
|
Validity Note
This documentation is valid for Harmony BX1 with the product version (PV) 02 or lower.
The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information.
Registered Trademarks
ARM, Cortex, and Cortex-A53 are registered trademarks of Arm Limited (or its subsidiaries).
Debian is a registered trademark of Software in the Public Interest, Inc.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.
Product names used in this manual may be the registered trademarks owned by the respective proprietors.
Related Documents
You can download the manuals related to this product, such as the software manual, from the Schneider Electric download center (www.se.com/ww/en/download).
Information on Non-Inclusive or Insensitive Terminology
As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.
Product Related Information
If the equipment is used in a manner not specified by the manufacturer, the protection provided by the equipment may be impaired.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Critical alarm indicators and system functions require independent and redundant protection hardware and/or mechanical interlocks.
When you cycle power, wait at least 10 seconds after it has been turned off. If this product is restarted too quickly, it may not operate correctly.
In the event the screen cannot be properly read, for example, if the backlight is not functioning, it may be difficult or impossible to identify a function. Functions that may present a hazard if not immediately executed, such as a fuel shut-off, must be provided independently of this product. The machine's control system design must take into account the possibility of the backlight no longer functioning and the operator being unable to control the machine or making mistakes in the control of the machine.
WARNING |
|---|
|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
For additional information, refer to NEMA ICS 1.1 (latest edition), "Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control" and to NEMA ICS 7.1 (latest edition), "Safety Standards for Construction and Guide for Selection, Installation and Operation of Adjustable-Speed Drive Systems" or their equivalent governing your particular location.
-
Operating System
-
Installed hardware
-
Installed software
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
EQUIPMENT DAMAGE
When powering off the product, use the shutdown command
to properly shut down the product.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
DANGER
WARNING