Performance Specifications
Processor |
ARM® NXP i.MX8M Plus Quad-Core |
Memory |
Onboard DDR4L 4 GB |
Storage |
eMMC 32 GB*1 |
Real time clock |
RTC x 1, with 3 V CR2032 Lithium battery*2 |
Operating system |
Debian 11 |
*1 The eMMC where the operating system is installed has a write lifespan. Although the eMMC is durable to handle data that is normally written in the system, continual write operations such as data logging will accelerate the end of the lifespan and lead to system failure. For continual write operations, such as data logging, write to a micro SD card or USB device.
*2 The expected battery service life is 7 years; however the battery may die before then. The battery is not user replaceable. Please contact your local distributor.
![]() |
---|
STORAGE DEVICE DAMAGE AND DATA LOSS
Use a Micro SD card or a USB device for continual
write operation such as data logging.
Failure to follow these instructions can result in injury or equipment damage.
|