EIO0000005096.04

Regular Cleaning

Cleaning This Product

NOTICE
EQUIPMENT DAMAGE
  • Power off this product before cleaning it.
  • Do not use paint thinner, organic solvents, or a strong acid compound to clean the unit.
Failure to follow these instructions can result in equipment damage.

When this product gets dirty, wipe with a soft, dry cloth or a soft cloth soaked in only water and wrung tightly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?