EIO0000005096.04

Cybersecurity Guideline

Use this product inside a secure industrial automation and control system. Total protection of components (equipment/devices), systems, organizations, and networks from cyber attack threats requires multi-layered cyber risk mitigation measures, early detection of incidents, and appropriate response and recovery plans when incidents occur. For more information about cybersecurity, refer to the Harmony HMI/iPC Cybersecurity Guide.
https://www.se.com/ww/en/download/document/EIO0000004948/

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords at first use to help prevent unauthorized access to device settings, controls and information.
  • Disable unused ports/services and default accounts, where possible, to minimize pathways for malicious attacks.
  • Close the ports that are not going to be used.
  • Disable or remove server services that are not going to be utilized.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Set sticky bit on all world-writable directories.
  • Restrict core dumps.
  • Ensure the syslog service is running.
  • Apply the latest updates and hotfixes to your Operating System and software.
  • Use cybersecurity best practices (for example: least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, interruption of services, or unintended operation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: For more details and assistance on how to apply the latest updates and hotfixes, please contact our customer support.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?