EIO0000005096.04

Part Number

Series

Part name

Part number

Harmony BX1

HMIBX1A0NDA

HMIBX1A0NDA

NOTE: This product has EcoStruxure Automation Expert Soft dPAC pre-installed. The supported version is 23.0. For the license activation of the software, please refer to the EcoStruxure Automation Expert documents on our website.
www.se.com/ww/en/download

LAN port settings to connect EcoStruxure Automation Expert Soft dPAC is as follows:

LAN2
IP address: 192.168.1.209
Subnet mask: 255.255.255.0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?