EIO0000005096.04

Connecting the DC Power Cord

DC Power Connector:

Connection

Wire

+

9...36 Vdc

-

0 Vdc

How to connect the DC Power Cord

  1. Loosen the screw on the product’s FG terminal, connect the grounding wire, and tighten the screw.
    NOTE: The necessary torque is 0.78 N•m (6.9 lb-in).
  2. Confirm the power cord is not connected to the power supply.
  3. Crimp a pin terminal properly to the end of each power cable wire.
  4. Push the opening button with a small and flat screwdriver to open the desired pin hole.
  5. Insert each power cord wire into its corresponding hole. Release the opening button to clamp the wire in place.
    NOTE:
    • When using stranded wire, do not short with neighboring wires.

    • When connecting with stranded wires, do not solder the stranded wires.

  6. After inserting the cord wires, insert the DC power connector into the power connector on this product.
  7. Affix the screws on both sides of the connector.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?