Parts Identification
|
1. DC power |
7. Reset button*1*2 |
|
2. HDMI port |
8. RS-232/422/485 port*3 |
|
3. USB 3.0 port |
9. Micro SIM slot*3 |
|
4. Giga LAN port |
10. Micro SD slot |
|
5. Indicators light |
11. Antenna x 3*3 |
|
6. CAN-FD port*3 |
12. Micro USB port*4 |
*1 Use of reset button may lead to system reboot and may affect system operation.
*2 To reboot the product, press the button 5 times in a row with the interval of less than 0.5 seconds.
*3 Not currently supported with the pre-installed version of EcoStruxure Automation Expert Soft dPAC. For the usage of these interfaces, please contact our customer support.
*4 Not currently supported and not for general purpose usage.
CAUTION |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Do not use the reset button until it is necessary.
Failure to follow these instructions can result in injury or equipment damage.
|
CAUTION