Interfaces
HDMI Port
The HDMI support port enables video output to an external display.
USB 3.0 Port
The USB 3.0 is a Type A connector, and can also support USB mass storage.
|
Power supply voltage |
5 Vdc |
|
Maximum current supplied |
900 mA/port |
|
Maximum transmission distance |
3 m |
WARNING |
|---|
|
EXPLOSION HAZARD
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Giga LAN Port
The standard RJ-45 LAN jack is provided the connection to the Local Area Network (LAN).
|
LED |
Function |
Status |
|---|---|---|
|
Yellow |
Active status |
ON: LAN link is established. OFF: LAN link is not established. Blink: Data received and transmitted. |
|
Orange/Green |
Link Speed status |
Green ON: 100 Mbps Orange ON: 1,000 Mbps |
LAN2
IP address:
192.168.1.209
Subnet mask: 255.255.255.0
CAN-FD Port
Provides two phoenix CAN Bus ports for external device connection.
|
System name |
Position |
Pin No. |
Definition |
|---|---|---|---|
|
can0 |
CAN1 |
1 |
H |
|
2 |
L |
||
|
3 |
GND |
||
|
can1 |
CAN2 |
1 |
H |
|
2 |
L |
||
|
3 |
GND |
-
CAN Bus Read/Write
-
The two ports can be connected each other as below:
-
The CAN-FD Port is connected to signals only. No external power load.
RS-232/422/485 Port
Provides two phoenix connectors for RS-232/422/485 interface.
|
System name |
Position |
Pin No. |
Definition |
||
|---|---|---|---|---|---|
|
RS-232 |
RS-422 |
RS-485 |
|||
|
/dev/ttym xc0 |
COM Port 1 (P1) (CN4) |
1 | - | TX- 1 | D- 1 |
| 2 | RXD1 | TX+ 1 | D+ 1 | ||
| 3 | TXD1 | RX+ 1 | - | ||
| 4 | - | RX- 1 | - | ||
| 5 | RTS1 | - | - | ||
| 6 | CTS1 | - | - | ||
| 7 | GND | GND | GND | ||
|
/dev/ttym xc2 |
COM Port 2 (P2) (CN5) |
1 | - | TX- 2 | D- 2 |
| 2 | RXD2 | TX+ 2 | D+ 2 | ||
| 3 | TXD2 | RX+ 2 | - | ||
| 4 | - | RX- 2 | - | ||
| 5 | RTS2 | - | - | ||
| 6 | CTS2 | - | - | ||
| 7 | GND | GND | GND | ||
-
For serial communication, the cable length must be less than 30 meters.
-
This interface is not currently supported with the pre-installed version of EcoStruxure Automation Expert Soft dPAC. For the usage of the interface, please contact our customer support.
Micro SIM Slot
User can insert the micro SIM card into the slot when using an LTE module via the mini card slot.
Micro SD Slot
Antenna
The three antenna configurations are Wi-fi, 4G or LTE.
Mini PCIe Slot
Internal Mini PCIe cards are not currently supported with the pre-installed version of EcoStruxure Automation Expert Soft dPAC. For the usage of the interface, please contact our customer support.
WARNING