EIO0000005096.04

Accessories

Products may change or be discontinued without notice. Please check our website for the latest information.
www.se.com/docs

Product name

Product number

Power Supply

Regulated Power Supply, 100-240 Vac, 24 V 1.2 A, single phase, Modular*1

ABLM1A24012

*1 Required to comply with IEC 61131-2, 61000-6-2 and 61000-6-4.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?