Installation Requirements
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
RISK OF BURNING INJURY
Do not touch the rear chassis during operation.
Failure to follow these instructions can result in injury or equipment damage.
|
-
Check that the ambient air temperature and the ambient humidity are within their specified ranges in Environmental Specifications. When installing this product in a cabinet or enclosure, the ambient air temperature is the cabinet's or enclosure's internal and external temperature.
-
Be sure that heat from surrounding equipment does not cause this product to exceed its standard operating temperature.
-
For easier maintenance, operation and improved ventilation, install this product at least 100 mm (3.94 in) away from adjacent structures and other equipment as shown in the following illustration: