EIO0000005096.04

Precautions for Building into an End-use Product

Be aware of the following when building this product into an end-use product:

  • The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.
  • Install this product in an enclosure with mechanical rigidity.
  • This product is an open type device and not designed for outdoor use. UL certification obtained is for indoor use only.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?