Environmental Specifications
|
Physical environment |
|
|
Ambient air temperature |
-10...55 °C (14...131 °F) |
|
Storage temperature |
-40...80 °C (-40...176 °F) |
|
Ambient air and storage humidity |
10...95% RH (Non condensing) |
|
Pollution degree |
For indoor use in Pollution Degree 2 environment |
|
Mechanical environment |
|
|
Vibration resistance |
IEC/EN 61131-2 compliant |
|
Shock resistance |
IEC/EN 61131-2 compliant |
Air Quality Requirements
Do not operate or store the product where chemicals evaporate, or where chemicals are present in the air:
- Corrosive chemicals: Acids, alkalines, liquids containing salt.
- Flammable chemicals: Organic solvents.
CAUTION |
|---|
|
INOPERATIVE EQUIPMENT
Do not allow water, liquids, metal, and wiring fragments to enter
the panel case.
Failure to follow these instructions can result in injury or equipment damage.
|
CAUTION