EIO0000005096.04

Micro SD Card Installation

CAUTION
STORAGE DEVICE DAMAGE AND DATA LOSS
  • Remove all power before making any contact with an installed storage device.
  • Make sure you regularly back up the data since storage devices have a life span and accidental data loss can occur at any time.
  • Confirm the storage device is correctly oriented before insertion.
  • Do not bend, drop, or strike the storage device.
  • Do not touch the storage device connectors.
  • Do not disassemble or modify the storage device.
  • Keep the storage device dry.
Failure to follow these instructions can result in injury or equipment damage.

To install an SD Card simply insert it into the slot on the side of the system as shown. Ensure the card is correctly oriented.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?