EIO0000003527.05

System Design

This section describes the system configuration with this product and peripheral equipment.

NOTE: The number of interfaces, such as serial and Ethernet interfaces, varies depending on the model. Refer to Parts Identification.

*1 In order to use this as an isolation port, Isolation Unit is required. To use RS-232C isolation unit, set the #9 pin of the COM port to VCC.

*2 Refer to Accessories.

*3 For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.

*4 HMIST6200 is not supported.

To use this product, transferring project data from the screen editing software is required. For details about transfer, refer to the software manual.
When transferring using the USB (micro-B) interface, connect cables in the following order:

  1. Attach the transfer cable to the USB (micro-B) interface of this product.

  2. Attach the power cable to this product, then connect the power cable to an external power source.

  3. Connect the transfer cable to the computer.

WARNING
UNINTENDED EQUIPMENT OPERATION
  • Do not connect the product to the computer with the USB (micro-B) cable unless the product is powered by the power cable.
  • Remove the USB (micro-B) cable before communicating with the host controller and other types of equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?