EIO0000003527.05

Serial Interface

Introduction

The serial interface is not isolated.

NOTE: For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.

On HMIST6200, you can switch the communication method between RS-232C and RS-485 via the software.

The SG (signal ground) and FG (frame ground) terminals are separated inside this product.

DANGER
ELECTRIC SHOCK
  • Make a direct connection between the FG (frame ground) terminal and ground.
  • Do not connect other devices to ground through the FG (frame ground) terminal of this device.
  • Install all cables according to local codes and requirements. If local codes do not require grounding, follow a reliable guide such as the US National Electrical Code, Article 800.
Failure to follow these instructions will result in death or serious injury.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use only D-Sub 9 pin cables with a locking tab in good condition.
  • Use a RJ45 connector that has a functional locking tab.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

HMIST6200 COM1 (RS-232C/485)

RJ45 connector

Pin No.

RS-232C/RS-485

Signal name

Direction

Meaning

1

RD (RXD)

Input

Receive data (RS-232C)

2

SD (TXD)

Output

Send data (RS-232C)

3

NC

No connection

4

D1

Input/Output

Transfer data (RS-485)

5

D0

Input/Output

Transfer data (RS-485)

6

RS (RTS)

Output

Request to send

7

NC

No connection

8

SG

Signal ground

Shell

FG

Frame ground

HMIST64/65/66/6700 COM1 (RS-232C)

D-Sub 9 pin plug connector

Product side:

Pin No.

RS-232C

Signal name

Direction

Meaning

1

CD

Input

Carrier detect

2

RD (RXD)

Input

Receive data

3

SD (TXD)

Output

Send data

4

ER (DTR)

Output

Data terminal ready

5

SG

Signal ground

6

DR (DSR)

Input

Data set ready

7

RS (RTS)

Output

Request to send

8

CS (CTS)

Input

Send possible

9

VCC

Output

+5 Vdc ±5% Output 0.25 A*1

Shell

FG

Frame ground

*1 When using RS-232C pin #9, enable VCC with the software.

Recommended jack screw is #4-40 (UNC).

HMIST64/65/66/6700 COM2 (RS-485)

RJ45 connector

NOTE: When setting up RS-485 communication, the cable diagram for some equipment may require polarization on the terminal side. Change the setting for polarization with your screen editing software.

Pin No.

RS-485

Signal name

Direction

Meaning

1

NC

No connection

2

NC

No connection

3

NC

No connection

4

Line A

Input/Output

Transfer data (+)

5

Line B

Input/Output

Transfer data (-)

6

RS (RTS)

Output

Request to send

7

NC

No connection

8

SG

Signal ground

Shell

FG

Frame ground

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?