EIO0000003527.05

HMIST6600

External Dimensions

1 Front

2 Left

3 Bottom

Dimensions with Installation Fasteners

1 Front

2 Left

3 Bottom

4 Top

Dimensions with Cables

1 Rear

2 Right

NOTE: All the above values are designed with cable bending in mind. The dimensions given here are representative values depending on the type of connection cable in use. Therefore, these values are intended for reference only.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?