EIO0000003527.05

Isolation Unit

You can install the Isolation Unit to the back of this product or to the installation panel. For details such as settings when using the Isolation Unit (XBTZGI232 or XBTZGI485), refer to the product manual.

DANGER
HAZARD OF ELECTRIC SHOCK OR EXPLOSION
Prior to connecting the Isolation Unit to this product, confirm that this product’s power supply is completely turned OFF.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?